This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8841: DRV8841 OCP issue

Part Number: DRV8841


Customer use DRV8841, meet OCP issue, the design follow DRV8841EVM. 

The max current through the motor is 1.3A, Risense is 0.36, Vref is 2.5V, so Ichop = 2.5/(5*0.36)=1.389A. 

Sometimes the motor will be locked, but the current is below 1A, and fault Pin output Low. Reset DRV8841 can work normal. the failure rate is about 2%.

Then we do another test, change the Risense to 0, test two days, don't repeat the issue. 

So we think the fault caused by OCP. 

Please provide more information, what condition will cause OCP, or OCP logic. thanks!

  • Hi Maka,

    Can you provide scope captures of the currents zoomed in to 5us/div showing 20us prior to nFAULT going low until 5us after nFAULT going low?

    Also, please provide similar scope captures of the outputs, nSLEEP, and V3P3OUT.