This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8881: PWM off time

Part Number: DRV8881

Hi,

 I do not understand clearly the specification of PWM offtime in the datasheet and specifically the logic low/logic high numbers that are typically 20usec/30usec.

How can they be consistent with an application that uses the driver at 100Khz(10usec period)?

Thanks

Umberto

  • Hi Umberto,

    In most use cases, the outputs can be set to a logic high or low and allow the DRV8881 to regulate the outputs.

    If an application is trying to PWM the inputs at high frequencies, the current regulation settings can adjusted such that it is not operating. This would allow the inputs to control the outputs.