Hello,
Regarding to IN1/2(logic input) on DRV8871, my customer is asking a question.
(Question)
・How is rise time and fall time in IN1/2?
I am understanding that generally, the maximum rise time and fall time of CMOS logic(Vcc5V) are approximately 20ns/V.
Is it same as above value?
They use very slow rise time and fall time(20us~) signal as IN1/2 and they are facing the anomalous oscillation on this device output.
Regards,
Tao2199