Hi Team,
May I know TI has function can compare Panasonic device AN44071? Also meet 1/256 microstep request.
I think use two Motor Driver implement is better. Could you help us to comment this? Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Cao Cao,
The closest matching device is the DRV8823, but it does not have 1/256 microstep.
If 1/256 is required, there are two choices. Use the DRV8711 or create your own pattern with the DRV8881E. In both cases, you will need 2 devices.