This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8711: Can the BoosterPack for it be used with MSP432P401R LaunchPad ?

Part Number: DRV8711
Other Parts Discussed in Thread: CC2564MODA

I have a project that needs Bluetooth communication.  I got  CC2564MABOOST-MSP432-BNDL: CC2564MODA BoosterPack + MSP432P401R LaunchPad. We also need to control two step motors. Can I just add two BOOST-DRV8711?

  • Hi Zhiyong,

    No you cannot just add two BOOST-DRV8711. There are two items to address:

    First there appears to be an issue using the MSP432P401R Launchpad that has not been resolved. See the thread e2e.ti.com/.../576971 for details.

    Second, each BOOST-DRV8711 should be written to separately. This means one SCS, STEP, and DIR pin per BOOST-DRV8711. The code would have to modified to account for this.