Hi all
Would you mind if we ask DRV2667?
We are considering the latency from input(analog or I2C) to output.
On your datasheet Figure 21. Front-End Interface P11, in case of I2C input(from RAM to Amplifier), how much is the latency?(less that 10ms or 1ms?)
There is the description "In the system application, the entire system latency must be kept to less than 30 ms total to be imperceptible to the end user".
So, we guess that it(latency) is less than 30ms at least.
Kind regards,
Hirotaka Matsumoto