This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8823: DRV8823 about single step function question

Part Number: DRV8823
Other Parts Discussed in Thread: DRV8821

Hi Team,

The customer would like to use DRV8823.

Q1: For the DRV8823, If the SPI bus is used to send the step commands, the main frequency of SPI is needed to increase at least 16 times 

at the same single speed. Is this understanding correct?

Q2: DRV8823 does not have the single step function pin. Do we have the single step function pin driving motor IC for the stepper motor?

Best Wishes,
Mickey Zhang
Asia Customer Support Center
Texas Instruments