Other Parts Discussed in Thread: DRV8301, DRV8301-69M-KIT
I am trying to run a Brushless DC motor rated for 34A using the DRV8301 and the gate current and gate voltage faults occur. Could this be a problem with the motor current rating? because the DRV8301 is only rated for 10A continuous output current with a 14A peak rating?