Other Parts Discussed in Thread: MSP430G2553
Hello ! everyone, I have some problem of DRV8307
According the DRV8307 EVM Schematic, I design the circuit to drive the BLDC Motor, like the picture below:
I use msp430g2553 I/O pin to connect to ENABLE,DIR,BRAKE pin,
and generate a 20KHz, duty 25% PWM to DRV8307 PWM pin.
start the motor, ENABLE = LOW, BRAKE = LOW,
stop the motor, ENABLE = HIGH, BRAKE = HIGH,
DIR = HIGH, The motor rotates Clockwise OK, the motor speed is OK
DIR = LOW, The motor rotates counterclockwise OK,but the motor speed is slow.
I read the datasheet, everytime start the Motor, Increase the PWM duty 1% to 25% slowly
But the problem is still the same.,Does anyone help me to figure out it ? Thanks