I am using the DRV595 to drive a 7V, 1A TEC and I have an overheating issue on a new project. The conditions are:
-
Power supply voltage of 7V
-
Ambient is 25C
-
Max TEC current is 1.1A (full drive)
-
According to those figures I should be dissipating only 0.13W across the two internal output transistors 1.1A x 1.1A x 60mOhms x 2
-
In theory, this gives me a temperature rise of only 3.3 degC above ambient
-
The layout of the PCB is according to the data sheet with thermal pad and thermal vias.
- The switching frequency is set to 1MHz
- The device works until it gets hotter (when fully driving the TEC) until it goes into the fault condition.
The symptoms are:
-
The DRV595 is going into FAULTZ condition and turning off the output
-
The temperature measured on the top of the package of the DRV595 is in excess of 60degC
Any ideas what is happening here or have I just got the math totally wrong!