Hi,
I'm looking for a driver to my application. I have to drive a 3-5A/12V brushed motor with 12A peak (150 ms). It seems both DRV8402 and DRV8432 is enough for me. My problem is putting it in a small board, so DRV 8432 should be better, because I can use a ferrite bead (BLM21PG220SN1D) instead of an inductor. Unfortunately, the inventory of this part at ti.com seem to be ZERO .
So, can I design my board to use a 8432 and, until I don't have it, can I use a 8402 instead? Is the ferrite bead enough?
Thank you
Adriano