Other Parts Discussed in Thread: DRV8302,
Hello sir,
I am using DRV8305-Q1 and DRV8302 to drive same BLDC motor. N-channel MOSFETs that is being used to supply current is same for two designs. PWM frequency used in both the cases is same that is 40kHz. I am using 28V supply for both the designs.
MOSFET part number: STL160NS3LLH7
But the problem is that my motor speed is slow with DRV8305-Q1 as compared to DRV8302.
I kept the IDRIVE to its maximum value that is 1.25A and 1A and observed that there is an improvement in slew rate (confirmed it by observing PWM signal at GHA i.e. pin 36 of DRV8305-Q1 and GH_A i.e pin 47 of DRV8302). I have also observed that slew rate for DRV8302 and DRV8305-Q1 is comparable when IDRIVE is max. But still I am getting poor response with DRV8305-Q1.
Ques1 : Is there anything that i should take into consideration to have a better response? If yes please enlighten me with all those factors that I should consider.
While comparing DRV8302 and DRV8305-Q1, I found that peak gate current for DRV8302 is 1.7A/2.3A while for DRV8305-Q1 is 1.25A/1A.
Ques2: Does this change in values of peak gate current will affect the motor performance? If yes please tell me the reason.
Quss3: Average gate current is same for both the devices right??