Hi
DRV10983 has flexible user interface and it is capable of 3 type of input to drive a motor (PWMin, analog and I2C).
How to express its resolution as N-bits?
BestRegards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Na na78,
The resolution is 9 bits.
Thanks,
Innocent
Hello,
Increase PWM input duty cycle and monitor phase voltage for increase in voltage. You have to increase PWM in smallest possible steps like 0.1% or lower and check for increase in voltage. The inverse of smallest PWM duty cycle change which causes increment in voltage is resolution (1/PWM duty).
Regards.
Krushal