This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/DRV8305-Q1EVM: Can not find all the lab projects in the motorware folder, specifically "proj_lab02"

Part Number: DRV8305-Q1EVM
Other Parts Discussed in Thread: MOTORWARE,

Tool/software: Code Composer Studio

Hi,

       I have recently purchased DRV8305-Q1EVM, I got proj_lab02b successfully running on this board. Now I want to control all of this using external potentiometer and as I see from motorware documentation that "proj_lab02d" is the program that provides all the control from user code. But I cannot find this project in the imported examples from motorware folder. I have following questions:

1. Where can I find "proj_lab02d" so that everything can be controlled from application code, or can someone direct me to material that will help me in achieving this?

2. I could not find a method or object that changes phase sequences for motor in "proj_lab02b". Please direct me to a library or function that is used for changing phase sequences for BLDC motor.

3. Is there is any material guide that can help in interfacing hall sensors and running motor using hall sensor feedback.

Any help with these questions will be greatly appreciated.

Eagerly waiting for your response.

Thank you!!