Other Parts Discussed in Thread: DRV8848
Hi,
DRV8835 is to reduce motor starting current.
As a measure to reduce the motor starting current,
we are considering changing the VM voltage (For example VM=3.0V → 7.0V).
1. Is this a problem as how to use DRV8835?
2. I can imagine that Ron of the built-in FET changes,
Is it possible to think that when the motor starts up, when the VM is low(For example VM=3.0V),
the current increases?
3. In addition to changing the VM, what is the best way to reduce the motor startup current?
best regards