This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8662: DRV8662 IC OVER HEATING

Part Number: DRV8662


Hello,

I had using the drv8662 ic for boost voltage 200vpp but when i turned on the supply the sw pin will get short to ground and draws maximum current eventually the ic become so hotter,

even though i  gave logic low to enable pin this will happens

i verified the circuit for short circuit but there is nothing

i had using the same circuit as recommended in datasheet pwm source is provided from arduino board

Thanks,