Other Parts Discussed in Thread: DRV8301, , DRV832X
Hello -
I have custom hardware utilizing TIs InstaSPIN technology and a DRV8301 gate driver currently (plus an external current shunt amplifier for full three-phase sensing).
I am looking closely at the DRV8323 as a potential replacement, as it has three current shunt amplifiers built-in. However, the current datasheet seems to have a couple inconsistencies. It labels the device as both "6 to 60-V" and "5.5 to 50-V". The maximum ratings state 65V for both the gate driver and the buck regulator.
Which is correct? My maximum input voltage is around 55V.
Any input is appreciated.
Thanks,
-asifjahmed