Other Parts Discussed in Thread: TIDA-00284,
What are the specifications to be kept in mind while designing a solenoid which is to be used with DRV110 to achieve target current consumption?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What are the specifications to be kept in mind while designing a solenoid which is to be used with DRV110 to achieve target current consumption?
I am trying to drive a solenoid with 167ohms DC resistance and inductance approx 322mH @10kHz. The minimum current that can be set with DRV110 is 35mA approx. I am unable to configure the same solenoid to consume 20mA.
Even if I increase to sense resistor to 2-3ohms from 1 ohm, the hold on current doesnt seem to reduce. Do I need to design a specific type of solenoid?