Hello, please find below my questions:
1.do you please confirm that this product http://www.ti.com/tool/drv8880evm can drive properly a stepper motor that requires 24 V input and 1.8 A? Regarding the current requirement I believe it is possible, but I would like to make sure that we don't have voltage output losses.
2.We will use an encoder on the motor and we need a pin dedicated for the interrupt from our linear encoder. in that case, could it be PIN 23?
3.Do you provide firmware or do we have to write everything from scratch?
4.Is this product CAN compatible or do we have to use CAN tranceiver?
5.Is this product ROHS, UL and EMC certified?
Thank you in advance.