This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV10975: VCC of DRV10975

Part Number: DRV10975

Hi all,

When DRV10975 writes data to EEPROM, does it need to input 22V to Vcc?

Recommended Operating Conditions of VCC is 18V(max).

However, when writing data to EEPROM, it is stated that it is necessary to input above 22 V.

Which is correct?

Best regards,

Sasaki