This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV595: Upcoming device planned for higher sink&source current?

Part Number: DRV595

Dear Team,

we were wondering if there are plans for higher-rated devices in the TEC controller portfolio.

Our customer was initially looking for a TEC controller with

  • Sinking capability of 10A @ buck mode
  • Sourcing capability of 5A @ boost mode
  • Vin_min = 24V

Option could also be a controller with external FETs.

Other ideas are also welcome.

Thanks for your feedback.

Best Regards
Martin