Part Number: DRV8837EVM
Other Parts Discussed in Thread: DRV8837
IN1 : PWM duty 80%, IN2 : PWM duty 0% / 400hz

Why is the IN2 and OUT2 different??
I think the back EMF is a problem... right?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DRV8837EVM
Other Parts Discussed in Thread: DRV8837
IN1 : PWM duty 80%, IN2 : PWM duty 0% / 400hz

Why is the IN2 and OUT2 different??
I think the back EMF is a problem... right?
Part Number: DRV8837
Hi
I try to use the coil with a PWM of motor drivers. But there are some problems.
I use stm32f1 MCU, IN1 : 80% 400hz, IN2 : 0% 400hz PWM
output of the coil is abnormal...When you see the picture, the signal of OUT 2 is not zero..
Normally, OUT1 is 80% PWM and OUT2 is near 0???
Why are IN 2 and OUT2 different??
![]()