I have Pin18 of the DRV8313 connected to ground - this pin was ground up till 2015 and is now reserved - i appear to be pulling current as son as Vm is 1V - is this expected or do i have another issue ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have Pin18 of the DRV8313 connected to ground - this pin was ground up till 2015 and is now reserved - i appear to be pulling current as son as Vm is 1V - is this expected or do i have another issue ?
Ian,
The datasheet has a revision where it changed pin 18 connection of the VQFN (RHH) package from GND to RSVD. This was due to a post similar to your thread here: e2e.ti.com/.../1839921 pin 18#1839921
So to answer your question, this pin should be left unconnected and not be tied to ground. Thank you.
Yes i realize that now - but question is what behavior should i expect to see id pin 18 is connected to ground ? ie will it cause high current to flow in device ?