This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8813: Decay mode at 0% Current Regulation

Part Number: DRV8813

Hi,

I need a clarification about the behavior of the driver when the bridge current is set to 0% by putting xI0=1 and xI1=1 and xENBL=1.

The datasheet says that the bridge is disabled: does this mean that all FETs are turned off and asynchronous fast decay will occur, or something else (i.e.: which is the decay mode in this condition)?

Thank you.

Best regards,

Marco