This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8801: DRV8801 Half bridge configuration

Part Number: DRV8801
Other Parts Discussed in Thread: DRV8816

Hello,

I have DRV8801 and I want use it to drive two half bridges instead of an H-bridge.

Is it feasible? I see there is only one PWM and it seems I cannot have independent PWM to control the two half bridges.

Thank you,

Fax