This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BOOSTXL-DRV8305EVM: BOOSTXL-DRV8305EVM - start with LaunchXL F28377S - no InstaSpin use

Part Number: BOOSTXL-DRV8305EVM
Other Parts Discussed in Thread: DRV8305, DRV8301, CONTROLSUITE

Hello,

I would like to extend my knowledge about the programming of BLDC motor control with the BOOSTXL-DRV8305EVM and wonder if there is somewhere source code or a tutorial that does not use InstaSpin controller ICs. I would like to use the Boosterpack with my F28377S Launchpad. It would be great if I do not have to start from scratch.

Is it useful to use examples from older, non-floating point controllers? Under the control suite, for example: HVMotorCtrl + PfcKit_v2.1 -> HVBLDC_Sensorless. However, this project is for a F28035 controller.

My main goal is to generate program code, which I can use on other controllers that do not have InstaSpin in the ROM.

I would be very happy about feedback and tips.
Many Thanks!