Other Parts Discussed in Thread: DRV8308, DRV8307
Hello
I have a 3-Phase, Sensor-less BLDC Motor powered from 24V supply. The motor can take 7A-10A of current during the acceleration. Steady state current is about 6A. The motor is capable of 20000RPM and I am running it at 10000RPM. I am looking for a stand alone driver that can be controlled preferably with PWM or analog input, speed and direction. I don't mind using external FETs. The closest I found is LV8907UW from ON Semiconductor. However, this controller is recommended for 12V applications. Does TI have a comparable chip rated for 24V?
Thanks,
Robert