This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8811EVM: Can not setup DRV8811EVM software - "Application cannot be started contact the application vendor"

Part Number: DRV8811EVM


Hi,

I cannot setup DRV8811EVM software .

I try it under win10 and under win7. The same error in both OS. Windows says "Application cannot be started contact the application vendor".

May be it is known bug?

BR, Oleg

  • Hi Oleg,

    We are not aware of any problems with the DRV8811EVM software.

    Are you referring to the USB driver or the Application?

    Prior to executing setup.exe, please set the compatability mode to Windows XP Service Pack 3. This has helped in the past.