Hello,
I am driving a 13V 13.2 ohm rotary solenoid using the DRV103.
My circuit is built on a surface mount prototype board. I do not have the thermal pad connected.
I was able to get the circuit working for a few times, but now when I apply power it drives the solenoid without the use of the switch on the Input pin.
The Status OK Flag is constantly low.
I believe that the part is now damaged which I did not think possible.
Are these symptoms of a damaged part?
Thanks,
Matt