Other Parts Discussed in Thread: DRV8307
Hello,
The DRV8308 and DRV8307 datasheets do not specify any tolerance for the CLK50 and TBLANK specifications; only the typical values are specified. I presume that the TBLANK time is based off of the CLK50 internal oascillator, so I can determine the TBLANK tolerance based on the CLK50 tolerance.
Is there any information available on the tolerance or range of CLK50 or TBLANK?
Thank you,
Jim