This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV10983: connect of motor temp sensor

Part Number: DRV10983


Hello,
customer needs to monitor the motor temperature. Is it possible to connect a temperature sensor to the DRV10983 in case he wants to run the DRV10983 standalone.

Regards, Holger

  • Hey Holger,

    While the DRV10983 does have the option to see if the junction temperature is over the "Shutdown Temperature Threshold" shown below, unfortunately, there is no way for the user to directly sense temperature using the device or attaching a sensor to the device.

    Would you like me to transfer this thread to temperature sensing forum?

    Best,

    -Cole