Hello All
I currently use an Allegro A4935 for a low voltage four quadrant control by using the same PWM signal for the PWMH and the PWML pins. This works well, however I now need to put a design together for a four quadrant control that works up to 54.6V (48V lithium battery). Does anyone have any idea;s how I can get the four quadrant working on the DRV8320 or similar that has a higher Vm?
Thanks