Part Number: DRV8308
I need to drive a 3 phase brusless DC motor of 100W at 12000RPM at constant load and need to be able to phase lock it with second motor with a tolerance of /- 5 degrees.
I've read in the datasheet of the DRV8308 that it is able to match the speed to a reference frequency on the CLKIN pin, but I can not find the accuracy of the speed nor phase error.
Are there any other parts or refence designs you can advise?
Thanks and best regards,