Part Number: DRV8323R
Other Parts Discussed in Thread: TMS320F28069, DRV8323
Hi,
I have two questions.
one is the juntion temperature and the other is BEMF.
1. Juntion temperature
I developed the board with DRV8323RH and TMS320F28069. And I succeed to control BLDC motor with 6-step and SVPWM method.
VM is 50V. When I enabled the DRV8323, the juction temperature rise above 80 degree in celcius. temperature was measured by thermal camera.
Is it OK? Although the operating range is upto 120 degree in celcius, I worry about the high temperature
2. BEMF problem
I use 50V power source. If motor generate the voltage over 20V by the external force, VM might be over 70V.
In the situation, DRV8323 can operate? all other parts such as MOSFET and capacitor are 100V standard.
I want to use DRV8323 which makes the simple schematic.
Thank you.