This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8800: Getting Vbb on both motor terminals V+ and V-

Part Number: DRV8800

Hello,

I would really appreciate some help. So I've connected DRV8800 driver by datasheet, but no matter how I connect pins nSleep, Enable, Mode or Phase, I always get Vbb on both motor terminals. I double checked the wiring and is okay. In datasheet the only possible scenairo is if the motor is in brake method.  I've tried all combinations but it doesnt work. This is now the second DRV8800 that's causing me the same problem.

It is kinda frustrating so any help would be very appreciated! :)

Regards,

Mitja