Hi,
two question regarding DRV8702D-Q1:
1) R(VDRAIN) 100-Ω series resistor (-> The R(VDRAIN) resistor should be used between the VDRAIN and VM pins to minimize current to the VDRAIN pin if no external reserve battery protection is implemented on the VDRAIN pin).
-> If there exists an inverse-polarity protection, can the resistor be left away? The inverse-polarity protection sits in the entry area of the electronics, not directly at VDRAIN.
2) Do you have details on the internal resistance pull down of the sleep pin?
Thx