Hi~ TI expert
I have designed a motor control board based on a DRV8701.
SO offset voltage(Voff) is fixed?
Voff range is shown in datasheet 50mV~250mV.
How can i know Voff value exactly? I used sensing resistor (10mohm)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Mason,
What value current are you trying to limit? What tolerance is acceptable?
Most motors do not need current limiting to be exact. There are tolerances throughout the system, such as VM, motor resistance and inductance, amplifier gain and offset, delays in firmware or hardware, and others that prevent accurate current limitation.