Hi,
My customer is using DRV8833.
Could you let me know the max/min value of current control PWM frequency, please?
Typ value is showd as 50kHz at Ta=25 in datasheet.
Customer wants to know the variation of this value.
The value is no problem by measured result of some samples.
Customer temp condition is -15~55 degrees.
Or Do you have data such as answer of this request?
If this variation is very big (ex: min 25kHz), this impacts to torque.
Best regards,
Shimizu