This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8307: BLDC starts and spins up to speed, but then shuts off and coasts

Part Number: DRV8307


The motor spins up and the 8307 outputs LOCKn. Then the device loses lock and coasts down to almost stopped. then it starts again on its own and repeats the process. These repeats until I stop the motor. The repeated stop and start produces excessive motor and FET heat.I am supplying a 20kHz PWM. I am using a 0.01 ohm R sense.