Part Number: DRV8818
Hello,
Our customer use the DRV8818, have a question.
Is mixed decay active at full step mode?
Best Regards,
Naoki Aoyama
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DRV8818
Hello,
Our customer use the DRV8818, have a question.
Is mixed decay active at full step mode?
Best Regards,
Naoki Aoyama
Hello James-san,
Thank you for your reply.
The customer have an additional question.
The customer have an issue of current control.
The configuration of the customer as follows,
Full step
mixed decay
VCC=3.4V and Vdecay=1.7V
C=470pF and R=33kohm placed at RCx
tOFF=15.51usec, tDF=2.83usec, tBLANK=0.658usec
SRn : L synchronous rectification
I attach the file their issue,
At first, it looks mixed decay is active. But after several msec, only slow decay is active.
When mixed decay active, a current is under control.
Do you have any idea?
Best Regards,
Naoki Aoyama
Hello Aoyama-san,
My guess is that because the current is increasing, mixed decay mode turns off. The datasheet says "Mixed decay mode is only used while the current though the winding is decreasing; slow decay is used while the current is increasing (p12)." Figure 7 in the application note "Current Recirculation and Decay Modes" shows that when current increases, slow decay is used, but when current decreases, mixed decay is used. In the customer's waveform, the DC current level seems to be rising to the set threshold.
What is the "Hold Indexer Mode" in the customer document that you sent? Is there a reason the customer needs mixed decay in this mode?