Hi there,
I have developed the Drive circuit for BLDC motor based on BOOSTXL -DRV8301.
I have successfully tested it and ran the motor identification lab2b and also lab11-lab11e(hall to fast).
Everything worked well, but suddenly it showed FAULTn .
I trapped the status register 1 which shows GVDDUV error - GVDD = 2.7V.
I had the same problem a few weeks before. Had to change the IC DRV8301.
But I would like to know why the fault occurs?
What could have possibly generated the fault of GVDD in IC?
In a bit time bound , Hope to get a response soon as possible.
Regards,