This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Control 350RPM Stepper Motor

Other Parts Discussed in Thread: TMS320F28069M, CONTROLSUITE

Is it possible to rotate a stepper motor at 350 rpm at 1/512 microstepping using tms320f28069m. If the answer is yes can anyone provide me supporting code. I use the PM_sensorless.c to achieve the target but at 1/512 microstepping maximum rpm is 3 and unable to increase ISR_FREQUENCY  beyond 23 khz.