Other Parts Discussed in Thread: DRV10983-Q1
Dear TI support team,
I have somes problems regarding the speed control via analog pot or pwm. I'm using the DRV10983Q1EVM to control the ec motor of a small fuel pump.
Speed control via I2C is working fine. But when I want to control the speed via the analog pot no matter which position the pot is in the ec motor rotates with a constant speed of ca. 3600 rpm.
when i check the OverRide box, I'm able to control the speed via I2C. This works perfectly fine. If I stop the motor here and discheck the OverRide box the ec motor doesn't start up again. Display looks the following:
As you can see the speed demand is roughly about 40 percent, but there is no voltage supply even though the power supply is still working.
To sum up: If the EVM is in analog speed control the ec motor spins with a constant frequency despite the analog pot voltage. (I measured the voltage of the pot and it works fine. ca. 3.3V at maximum)
This whole problem occured after I used the EVM with pwm speed control. First it worked fine. Then I changed the pwm source and it stopped working. Since then I have the aboved mentioned problems.
Hope you can be of some assit.
Regards
Alexander