Part Number: DRV8432
I want to use the DRV8432 to control the motor in Parallel Full Bridge Mode.As it is shown in datasheet figure 15.But I dont know the relation between PWM_A and PWM_B,are they complementary?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DRV8432
I want to use the DRV8432 to control the motor in Parallel Full Bridge Mode.As it is shown in datasheet figure 15.But I dont know the relation between PWM_A and PWM_B,are they complementary?
Hi wei liu62,
What M3, M2, M1 settings are you using?
Please refer to section 7.4 of the datasheet for details.