Hi ,
I am using DRV11873 to drive the color wheel motor on our projector project.
I needs a constant and stable rotating speed to protect the color wheel motor. so,I detect the pin of FG to get the rotating speed of the color wheel motor.
The attach is the schematic .
Through observing oscilloscope ,I found out the sudden change of FG signal in a few hours .
The FG frequency change dramatically In two seconds,then turn into normal frequency .
The attach is the FG and RD waveform of two circuit boards.
Oscilloscope channel 1 and channel 4 represents the RD signal.
Oscilloscope channel 2 and channel 3 represents the FG signal.