This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8704: UVLO bit

Part Number: DRV8704

Hello,

Our customer use the DRV8704, check the UVLO function.

When the voltage of VM falls below the UVLO threshold, it stops all FET, UVLO bit is set and nFAULT pin is Low.

The customer confirmed that it's operate correctly. 

When the voltage of VM rise above UVLO threshold, operation resume and nFAULT pin is High, but UVLO bit is

not clear.

Does it need to write '0' to UVLO bit for clear?

It is mentioned UVLO bit is Read only on the datasheet.

Best Regards,

Naoki Aoyama