This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMD18200: Specifications

Part Number: LMD18200

Good day,

I would like to inquire on the following specifications of LMD18200:

1. Saturation Voltage (upper and lower side)

2. over current protection circuit (description)

3. rush current protection circuit (description)

4. minimum pulse width of IN1 and IN2

Thank you.

  • Hi Joseph,

    Please point to the section of the datasheet for each specification you want? Thank you.

    Also, we have newer devices that may meet your needs. Can you provide a little information, such as:
    the system voltage
    the current needed
    the protection features
    your application
  • Thank you for your response.

    This defines the specifications that I need:
    1. For the saturation voltage, it is usually found in the electrical characteristics.
    2. Over current protection - if there is a built-in circuit, how much of a current will there be before shutdown?
    3. rush current protection - when switching, stop mode should be entered
    4. minimum pulse width - no need since it was stated in the electrical characteristics.

    For the suggested newer devices, what we need are as follows:
    1. System/supply voltage - greater than 17 volts
    2. output current - 1A (Peak) is enough
    3. built in diode
    4. Built-in over current protection, over temperature protection, and rush current protection
    5. Minimum Input operating voltage - 2.0V
    6. Saturation Voltage
    7. Diode Forward Voltage
    8. Minimum input pulse width - less than 8ms

    Thank you for your support
  • Good day,

    I would like to ask for an update regarding this enquiry. This item is a candidate as a subpart for TA7291P (TOSHIBA), and for it to be evaluated we need to complete the specifications first.

    If there are newer devices that are compatible with the said item, we would like to know their specifications too.

    Thank you very much.