This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I have a few questions regarding the recording attached
1. Is situation that RESET ,A,B,C are high can cause damage to DRV8312 even when the PWM lines are low
2. this is my PWM signal (the motor rotate) is this situation normal when PWM A,B are simultaneously high, or could it cause damage to DRV8312
because this situation differs from the PWM in the data sheet - PWM A inverted from PWM B
best regars
noam
Hi Rick
I saw 5 times damage to one of the DRV8312 phase. I don't know what Cause the damage this is my problem.