Other Parts Discussed in Thread: UCC27517
Hello,
I'm driving a solenoid on a 12-24V DC supply with the DRV110 as a PWM source driving into a UCC27517 Gate Driver. During cycle testing the PWA has been failing repeatedly. Each time it appears to be related to a drop in peak current. On some boards, replacing the Rpeak resistor has resolved the issue. On others it does not. The waveforms look correct, with the duty cycle changing between peak and hold correctly, and the hold current is correct. However the value read on a DMM for the Rpeak is showing ~40-42k Ohm depending on the unit when the value is in fact 100k. The reading across Rhold is ~420k Ohm which is correct. The resistor at Rpeak reads correctly at 100k when removed from the board and the resistance between the Rpeak pin and ground is ~50M Ohm when the resistor is removed. The PWA sits on top of the solenoid piston and coil so is subject to some impact vibration, though it is isolated from most of that shock. I am unable to figure out why my Rpeak value is shifting, and almost always down to the same ~40k level, after cycling for a while (8-12 hours). Is it possible something in the IC could drive this change in resistance reading?