Other Parts Discussed in Thread: DRV8308
We are going to use drv8308 for a blower driver. We connect motors as show in their datasheet, enable EVM board, give PWM. According to motor behaviour(either rotates fine or jitters) we choose halpoll 1 or 0 and then adjust Advance parameter to get a trapezoidal shape phase voltages (which also reduces current reading).
The problem is we are getting different results for different motors. Even though we have seen the phase voltages are trapezoidal, we do not get a good performance for some blowers ( not good because flow and pressure readings does not match their datasheet).
For example micronel blower data sheet we suppose to have 400 l/min flow but we read 160 l/min.(The problem is not specific to this motor)
dataseet http://www.micronel.com/uploads/tx_micronel/U71MX-tec.pdf
We have tried four different blowers and 2 of them we get readings which matches datasheet and 2 of them does not. What can be the reason for this? How to resolve this issue?
We have also tried sine commutation and the problem remains.